I am running the HV kit PMSM code for the 28335 on an EZDSP 28335 board. I am now up to build level 5. When I run it is current loop mode, it works fine. When I switch to speed loop mode, It seems to wor OK also. The problem is if I change to a negative speed ref, the instantly stalls and oscillates with a very high pitch (very loudly). I would appreciate any suggestions on probably cause.
Thanks,
Brad Mularcik