Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Hello,
we produce servo drive based on F28377s. The software is based on the IDDK exemple.
Now, we want add the Biss/Endat possibility.
To do this, we will use the TI Biss and endat library which use the CLB.
As I seen on this forum (10 september), datasheet was updated to explain the CLB and a configuration tool will coming soon.
I just seen the CLB block is not available on F28377s, but only on the F28379s.
-1) Is F28377s software and hardware are fully compliant if we replace the microcontroller by a F28379s? (CCS IDE project option need change target from 77 to 79, but it is the only change to do?)
-2) Biss/Endat library exemple are given for the F2837xD. I think the library work also on the F28379S version?
Thenk