Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE, INSTASPIN-BLDC
Driver is not provided with the USB stick included in the development kit.
Viewing in the device manager, the entry is marked with an exclamation mark, installing drivers e.g. from controlSUITE gives an error message as follows:
“Windows has found a driver for the device, but an error has occurred: Texas Instruments XDS100 Version 1.0 B”, “The has value for the file is not available in the given catalogue file. The file probably is defective or modified illegally.
Starting the program “InstaSPIN-BLDC_GUI_DRV83xx_v104.exe”, following error is shown:
“VCP auto-connection is enabled for this interface but no ports are available”.
It runs “disconnected”.
Using the Connection wizard as indicated results in the error message:
“Unable to connect to the selected target, please verify that the target is available and ready to receive connections.”
Best would be sending me the needed Driver or giving me the link where to find it.
Thank you and with Kind regards,
Carl.