Part Number: TMS320F28374S
Hi,
Just one question about SCI boot1.
Is it possible to use SCI boot1 (GPIO28/29) as the default option, without changing the OTP registers through JTAG?
Thanks a lot.
Br, Jordan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28374S
Hi,
Just one question about SCI boot1.
Is it possible to use SCI boot1 (GPIO28/29) as the default option, without changing the OTP registers through JTAG?
Thanks a lot.
Br, Jordan
You can configure EMU_BOOTCTRL @ 0xD00 to select boot modes while JTAG is connected.
But for the boot to pick SCI boot1 option without JTAG, you need to configure OTP settings.