Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Hello
I use the SPI(a) with an external FRAM, then I set the LSPCLK to 200MHz instead of 50MHz to reach speed up to 50MHz on Memory clock.
Now, on other SPi (b), I want drive an SSI feedback.
But some feedback has maximum clock frequency to 1Mhz..
But with LSPCLK which applied to all SPI, the minimum SPI clock is 200MHz/128 = 1.5625.
To have lower clock, I must reduce the LSPCLK, but this impact the memory clock frequency.
Is there some solution to keep an SPI at 50MHz and an other lower than 1MHz?
Thank