This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When we try to load program, read or erase from the Uniflash gui, we get an error saying "spawn unknown".
We tried running dslite.bat and got a Windows error saying that the version of dslite.exe we were running is incompatible with the version of Windows in use.
I have the gui log file, but I cannot fond a ds.log file on the pc.
Contents of gui error log;
13:10:30:210 log - NWAgentAPI: dinfraConfigue resolved successfully.
13:10:30:939 error - {}
13:10:31:006 error - {}
13:10:31:058 error - {}
13:10:31:068 error - {}
13:10:31:136 error - {}
13:10:31:173 error - {}
13:10:31:249 error - {}
13:10:31:257 error - {}
13:10:31:299 error - {}
13:10:31:317 error - {}
13:10:31:339 error - {}
13:10:31:356 error - {}
13:10:34:262 error - {}
13:10:34:265 error - {}
13:10:34:394 error - {}
13:10:35:256 error - {}
13:10:53:140 error - {}
13:10:53:190 error - {}
13:10:54:585 error - {}
13:10:54:812 error - {}
13:10:54:845 error - {}
13:10:55:163 error - {}
13:10:55:351 error - {}
13:10:55:356 error - {}
13:10:56:211 error - {}
13:10:56:232 error - {}
13:10:57:319 error - {}
13:10:57:333 error - {}
13:10:57:334 error - {}
13:11:00:229 error - {}
13:11:00:232 error - {}
13:11:00:868 error - {}
13:11:00:872 error - {}
13:11:04:639 error - {}
13:11:24:207 debug - Target Configuration. Device: f28m36p63c2, Connection: TIXDS2XXUSB_Connection, LP: false
13:11:24:834 debug - ufDS, session.configured, partnum of current session = f28m36p63c2
13:11:24:911 debug - addTargetStateListener on Cortex_M3_0
13:11:24:911 debug - addTargetStateListener on C28xx_0
13:11:25:070 error - {}
13:12:19:092 debug - returning new configure
13:12:20:575 error - {"message":"spawn UNKNOWN"}
13:12:20:575 error - configure failed: spawn UNKNOWN
13:12:20:575 error - {"message":"spawn UNKNOWN"}
13:12:20:576 error - spawn UNKNOWN
13:13:54:653 error - {}
13:14:05:143 debug - returning new configure
13:14:05:170 error - {"message":"spawn UNKNOWN"}
13:14:05:170 error - configure failed: spawn UNKNOWN
13:14:05:170 error - {"message":"spawn UNKNOWN"}
13:14:24:501 debug - returning new configure
13:14:24:538 error - {"message":"spawn UNKNOWN"}
13:14:24:538 error - configure failed: spawn UNKNOWN
13:14:24:538 error - {"message":"spawn UNKNOWN"}
13:14:24:538 error - spawn UNKNOWN
13:14:36:603 error - {}
13:20:27:306 debug - returning new configure
13:20:27:335 error - {"message":"spawn UNKNOWN"}
13:20:27:335 error - configure failed: spawn UNKNOWN
13:20:27:335 error - {"message":"spawn UNKNOWN"}
13:20:37:670 debug - returning new configure
13:20:37:704 error - {"message":"spawn UNKNOWN"}
13:20:37:704 error - configure failed: spawn UNKNOWN
13:20:37:704 error - {"message":"spawn UNKNOWN"}
13:20:37:704 error - spawn UNKNOWN
13:20:48:409 error - {}[quote user="Andy Faithfull1"]
Andy,
Which version of UniFlash are you using?
Do you know that the latest UniFlashV5.1 is supported only on 64-bit Windows 7/8/10?
Please check if you are using it on a 32-bit Win OS.
Thanks and regards,
Vamsi
I think (I will need to check) that we are using version 5.0.
Is there a 32-bit version that supports the device we are using (F28M36P63C2)?
Best regards,
Andy
Andy,
UniFlash4.6 supports Win32.
http://software-dl.ti.com/ccs/esd/uniflash/docs/release_archive.html#uniflash-v4-releases
Thanks and regards,
Vamsi
Many thanks Vamsi.
I have downloaded the installer, and I will update the ticket as soon as I have tried it out.
Best regards,
Andy
Andy,
You are welcome. Did you check whether you are using Win32 or Win64?
Thanks and regards,
Vamsi
Hi Vamsi,
We are using Win32.
All OK now, we have Uniflash v4.6 installed and working.
Many thanks,
Andy
Andy,
Glad V4.6 worked.
FYI for others that may visit this post: UniFlashV4.6 is the last build that supports 32-bit Windows. UniFlashV5.X and onwards support only 64-bit Windows.
This detail is mentioned in the release notes.
Thanks and regards,
Vamsi
Hi again Vamsi,
I have had some difficulty generating the stand-alone command line files.
Sometimes the batch file for the C28 core does not contain the name of the file to load. Also, when we want to load binary files, the start address we enter (in the gui) does not get written to the batch file. The start address is always written as 0.
Is this known behaviour?
Best regards,
Andy
Andy,
Please start a new thread so that the subject helps others as well.
Thanks and regards,
Vamsi