This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Confusing on example code C2000Ware - v:2.00.00.02

Part Number: TMS320F28379D


Tool/software: Code Composer Studio

Hi there,

I am quite new on CCS. I am using LaunchPad XL TMS320F28379D. I use the "Resource Explorer" to get the examples, CCS\Project\Example...

I have done the simple "ipc_gpio_toggle" project. I am going to test the IPC driver to transfer data between two CPU. But the example projects make me confusing.

As shown on the following picture (from Resource Explorer), there are two project name "cpu01_to_cpu02_ipcdrivers_cpu1" but no project name "cpu01_to_cpu02_ipcdrivers_cpu2" exits.

The same occurs on the projects "cpu01_to_cpu02_ipcdrivers_lite" and "cpu01_to_cpu_02_ipcdrivers_wprotect".

I have tried downloading the two projects name "cpu01_to_cpu02_ipcdrivers_cpu1" to my workplace, the main file is "cpu01_to_cpu02_ipcdrivers_cpu02.c" and the setting for this project is for the CPU2 in both projects.

Are they mistakes? Could you please give me detail advice to run these projects for the ipcdriver?

Kind Regards,

Alex