This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNIFLASH: Image is sometimes missing when using Uniflash to generate Standalone command line package for a dual-core device

Part Number: UNIFLASH

We are using Uniflash to program F28M36 devices.

Sometimes when generating a standalone command line programming package, the image for the slave (C28) core is not added to the zip file.

We have worked around this by manually adding the user_files\images folder and the relevant .out file.

Also, when loading binary files, the start address entered by the user is ignored, and the value written into the programming batch file is always 0.