Could someone at TI please file a bug report to fix typos in SPRU430E? I've been keeping a running tab, & have found a bunch so far:
2-25 to 2-31:
table heading "Affect of or Affect on C" should be "Effect of or Effect on C"
table heading "Affect on the TC bit" should be "Effect on the TC bit"
"OCV" should be "OVC": 6-36, 6-37, 6-38
D-7: SPAC translates to "SUBL ACC,P<<PM" (shown incorrectly as "SUB ACC,P<<PM")
5-27: there is no TH; "@TH" and "TH" should be "@T" and "T" respectively (although see p. B-4)
6-157: MOV ACC,#16bit<<#0..15 takes an immediate constant, but the SYNTAX OPTIONS shows a loc16
6-178: "MOVL PL, loc16" under SYNTAX OPTIONS should be "MOV PL, loc16"
6-207: "Greater Then" and "Less Then" should be "Greater Than" and "Less Than"
6-239: (MPYU) Description uses the word "signed" twice; these should read "unsigned"