Part Number: TMS320F28027
Tool/software: Code Composer Studio
Hello,
I want to create three EPWMs corresponding to two duty cycles, D1 and D2; the third duty is 1-D1-D2. All of them must be synchronized. The figure below shows how I am implementing it currently. A rising edge delay is also provided for each EPWM to implement dead time between the signals.
Question: is this is the best way to implement it? In future, I also plan to incorporate HRPWM into the scheme. Would that create a problem?