Hi,
I'm using the Renewable Energy Kit with an TMS320 F28035 DSP and the Blackhawk USB2000 Controller. I wanted to built a basic setup with an emtpy main( ) routine, just to get a starting bundle with all important files.
I used the 2803x C/C++ Header Files and Peripheral Examples Quick Start document and did the setup as told.
Included are the files shown in this picture
I'm not sure about which cmd file I should use, because there are the F28035_lnk.cmd and 28035_RAM_lnk.cmd files
At the moment I get this console output:
**** Build of configuration Debug for project Basis ****
D:\Programme\Texas Instruments\ccsv4\utils\gmake\gmake -k all
'Building target: Basis.out'
'Invoking: C2000 Linker'
"D:/Programme/Texas Instruments/ccsv4/tools/compiler/c2000/bin/cl2000" -z -m"Basis.map" --warn_sections -i"D:/Programme/Texas Instruments/ccsv4/tools/compiler/c2000/lib" -i"D:/Programme/Texas Instruments/ccsv4/tools/compiler/c2000/include" --reread_libs --rom_model -o "Basis.out" "./basis_main.obj" "./DSP2803x_GlobalVariableDefs.obj" -l"rts2800_ml.lib" "../28035_RAM_lnk.cmd" "../DSP2803x_Headers_BIOS.cmd"
<Linking>
This application has requested the Runtime to terminate it in an unusual way.
Please contact the application's support team for more information.
warning: creating ".stack" section with default size of 0x400; use the -stack
option to change the default size
"../28035_RAM_lnk.cmd", line 118: error: run placement fails for object
".stack", size 0x400 (page 1). Available ranges:
RAMM1 size: 0x380 unused: 0x380 max hole: 0x380
"../DSP2803x_Headers_BIOS.cmd", line 101: warning: memory range not found:
PIEVECT on page 1
"../DSP2803x_Headers_BIOS.cmd", line 101: error: run placement fails for object
"UNION_1", size 0x100 (page 1)
build.c:1949:internal fatal error #10251:
("EmuKeyVar:DSP2803x_GlobalVariableDefs.obj")
INTERNAL ERROR: D:\Programme\Texas Instruments\ccsv4\tools\compiler\c2000\bin\lnk2000.exe aborted
This is a serious problem. Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.
>> Compilation failure
D:\Programme\Texas Instruments\ccsv4\utils\gmake\gmake: *** [Basis.out] Error 1
D:\Programme\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.
Build complete for project Basis