Part Number: TMS320F280049C
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 8.2.0.00004)
I get the above error when I try to load code into the the TMS320F280049CPZS control card which is placed on the controlcard docking station.
And the D1 LED on the control card is flickering instead of a solid ON.
Is there a hardware problem?
I have another control card which I am able to power and debug without any problem.