This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: TMS320F280049C

Part Number: TMS320F280049C


I am using TMS320F280049C launchpad. It's using XDS110 to flash code and debugging. Suddenly It stopped flashing and give error as shown below.

Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 8.3.0.00003)

I have 2 launchpads and another is working fine with the same cable and setup files. can the issue be with JTAG controller or else?