This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: IBIS Model Question

Part Number: TMS320F28375D

Team,

Pins E18 and E19 seem to have some undocumented functionality.  

It seems that maybe these were intended to be a second USB port or something. 

If I then look at the GPIOUSBV4_NFS_7LM model there are several options for the I/O configuration.

Which of these is the C2000 using as the I/O configuration if  using these pins as EMIF address lines A7 and A8?

Thanks,

Andy