This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: C2000-GANG OTP ADDRESS

Part Number: F28M35H52C


I have been on vacation since September 28th, so I was unable to respond to you in time. After using the beta version, I found that the following problems still exist.

1 Now the OTP programming address range in the Memory Option can indeed contain 0x680800, but after clicking the Open code file in the software and selecting the file with this address, it will still report that 0x680800-0x680804 is out of range.

2 The 28M35 M3 core has a program burning problem. If you burn a code file without a CSM password, you can burn it all the time. If you burn a code file with a CSM password, you can only burn it once in the first time without a password, and then you won't be able to burn it.