Other Parts Discussed in Thread: TMS320F28335
If I use the McBSP in SPI mode on an tms320f28335, is my max data rate 25 Mbit/sec, or is there some other limit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F28335
If I use the McBSP in SPI mode on an tms320f28335, is my max data rate 25 Mbit/sec, or is there some other limit?
Paul,
In master mode, yes, this is true - and the 25 MHz limit is driven by the I/O output buffer speeds.
In SPI slave mode, the McBSP is limited in that CLKX has to be a minimum of 8 CLKG ccles (where CLKG = LSPCLK/2, and the maximum LSPCLK = 75 Mhz).
Therefore the maximum CLKX speed in slave mode is LSPCLK/16 = 4.6875 MHz.
Paul -
No, the dedicated SPI port has the following speed limitations:
Master mode transmit 25-MHz MAX, master mode receive 12.5-MHz MAX
Slave mode transmit 12.5 -MHz MAX, slave mode receive 12.5 -MHz MAX.
All of the above information is available in the Electricals section of the device data sheet (look under Electrical Specifications -> McBSP Timings -> McBSP as SPI, and Look under Electrical Specifications ->SPI Timings)