Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE
Is it possible to do Sensored Field Oriented Control in DRV8312-C2-KIT ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE
Is it possible to do Sensored Field Oriented Control in DRV8312-C2-KIT ?
It supports QEP encoder for sensored-FOC. You may find such sensored-FOC example in the below folder, which is easily ported to the DRV8312-kit though the example is based on HV-Kit. You just need to change the device configuration without changing the FOC algorithm.
C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1
Thank you for the response,
Actually, in controlSUITE They provided only source code for sensorless FOC of PMSM.
No sensored-FOC for DRV8312-C2k_kit, but there is a reference code for High voltage kit as I mentioned above, you may refer to the reference and port it to DRV8312-kit if you want, which should be easy to do by yourself.