Part Number: TMS320F28377D
Tool/software: Code Composer Studio
Hi,
I designed a board using the F28377D dual core device and I am currently trying to get any one of the sample codes from the C2000 ware for the single core to work on the device.
The program compiles (even though it reports that __disable interrupts() function doesnt resolve as well as memcpy is not defined).
I am able to connect to the device and download the code. The code runs to main and it fails in the InitSysCtrl(); function.
I have seen other folks had similar issues but didnt see a clear resolution for the problem. The screenshot is attached below.
I am using the XDS200 JTAG emulator with 14 pin connection. The boot mode is set in Get mode (but is that important in JTAG emulation).
Looking forward your support.
Thanks
Jay