This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: The internal circuit diagram of ADC input PIN required

Part Number: TMS320F28069M

Hi team

          My customer uses the internal ADC of TMS320F28069M to monitor the DC BUS voltage, but the voltage of the ADC input pin just reached 3.9V when he short circuited the external resistor for experiment. So he wanted to check the  internal circuit diagram of ADC input PIN to see if there is any clamp circuits.

Best Regards,

Wesley Huang

 

Field Application Engineer,China

Texas Instruments Semiconductor Technologies (Shanghai) Co., Ltd, Guangzhou Branch

Cell : +86-189-2449-8998

Email: wesley-huang@ti.com