We're seeing a very strange problem on a 28335. We have code in external RAM loaded in through the debugger. In one spot, when we open the code space in a memory window in the debugger, we see one location which shows a different value when we switch from Program space to Data space. It appears that at this location the memory access reads/writes a different memory location for Program and Data space. We can write a value into each location and it stays there. So, for example, we can set the window to Program space and write a 0x1111, then change to Data space. In Data space we see some other value. We then write a 0x2222 to Data space and it sticks. If we then switch to Program space, that location shows 0x1111 and when we switch back to Data space it shows 0x2222. All of the rest of the memory in that area acts as you would expect -- Program and Data space are the same.
Any ideas what could cause this? It is also repeatable between boards, so it isn't a broken processor or memory chip. It also effects real code -- we found it because we were doing an AND of 0x00FF with data, and the 0x00FF was being pulled from Data space (apparently) and so it was getting 0x1275 (or something like that). When we change the 0x1275 to 0x00FF it works, but we can't really do that.
Dave