Hello,
My customer asked if a 1.8-V external oscillator
can be connected to the X1 pin of F28027.
Is it possible and guaranteed ?
Thanks and regards,
Kazuaki Ohshita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My customer asked if a 1.8-V external oscillator
can be connected to the X1 pin of F28027.
Is it possible and guaranteed ?
Thanks and regards,
Kazuaki Ohshita
Kazuaki Ohshita said:Hello,
My customer asked if a 1.8-V external oscillator
can be connected to the X1 pin of F28027.Is it possible and guaranteed ?
Thanks and regards,
Kazuaki Ohshita
On 2802x this pin is for the internal on-chip oscillator input only. Please refer to the pin descriptions in the data manual:
On-chip crystal-oscillator input. To use this oscillator, a quartz crystal or a ceramic resonator must be connected across X1 and X2. In this case, the XCLKIN path must be disabled by bit 13 in the CLKCTL register. If this pin is not used, it must be tied to GND.
-Lori
Lori-san,
Thanks for your reply.
I understand.
Thanks and regards, Kazuaki Ohshita