This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can you help me a blinkled example code for LF2406A

Hi everybody,

I want to check running ability of my chip ( TMS320LF2406) . I want to try writing a blinkled example.

I  had a example for 2407A, repaired main code and CMD file  a little to conform 2406 memory map. I compiled ok, But I didn't download example code to chip  ( although I completed the downloading 2407A out code to it )

Programmer warns follow :

>>>> Begin Clear Flash Operation
Clearing 4 sectors in progress...
..Clear operation - OK (4 seconds)
<<<< End Clear Flash Operation
>>>> Begin Erase Flash Operation
Erasing 4 sectors in progress...
Erase operation - OK (1 seconds)
<<<< End Erase Flash Operation
>>>> Begin Program Flash Operation
Program in progress...
Programming at 0x1000 ..ERROR: Cannot read user code from section 3
<<<< End Program Flash Operation

>>>> Begin Verify Flash Operation
Verify in progress...
ERROR: Cannot read user code from section 3
<<<< End Verify Flash Operation

What is the problem in my example code ? 

Can you help me an blinkled example for 2406A ? 

7065.test240x.rar