This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: I want higher peak current on mi PMSM Motor on speed control to have a faster response. Also I can't achieve the target speed with the load(propeller) causing not be able to get more thrust.

Part Number: TMS320F28027F


I'm applying a Step of the maximun speed to see the response. 

I tried change the  USER_MOTOR_MAX_CURRENT      but this not solved it. 

I tried change The speed PID , acceleration  and the current increases a little bit. 

In the first tests  I saw 30A in the rail and changing the speed PI I saw 35-37 in the rail. I want the double!!!!

Increasing  USER_MOTOR_MAX_CURRENT  I didn't saw any changes, until I increase like 3x the motor got unstable.

I'm working on lab05.