Part Number: TMS320F28376D
Other Parts Discussed in Thread: C2000WARE
Hi everybody ,
I m on F28376D . I m for legacy on C2000ware 1.00.06.00 and CCS 8 .
now I write flash and need to read back fro cross check .
my programs hangs after reading about 90 words ( i tested the same moving starting writing locations ) : what I read and see in my variable is 0x0D00 vs correct value which is 0x8D00 .
issue I see is that memory view confirms me locations is properly written ( in there I see proper value 0x8d00 ) .
see attched picture with highlighted in red the memory view and the variable with the mismatch .
where am I wrong ? what should I check ?
I am using API and put some extra Nop in flash . I started from C2000 ware example so not touching any flash settings .
best regards
Carlo