This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Replacement 20 pin ribbon cable for XDS110 Debug probe

Hi,

We have a couple of XDS110 whose debug ribbon cable seems to be damaged. I have tried using a cable from a new XDS110 witg our older XDS110s and they are debugging fine. Is there a part number for this type of ribbon cable a so that we can order spares on Mouser. i have looked at the connectors without cables on mouser but there are many variants. 

The end of the cable which goes into the jtag is a 20 pin IDC connector with 1.27mm pitch. If i know the other end connector it will solve the problem.