Hello,
I'm using a custom board with F28332. On previous device i used F28335 with same program. Now I am getting some hardware mistakes (I hope that they are hardware).
Sometimes DSP reboots without any reason during work and it happens in random time. I've disabled WD, so it cant be it's work.
Sometimes during loading code CCS says - data verification failed during loading at address 0x8xxx (I saw it at two different addresses). I switched boards (so DSP's too), but errors dont stop. It's RAM, so this error is really serious. When I load my code in flash and start from it, it will copy some functions to flash, and what if it copies them with errors?
Yesterday my program wrote dummy data in one of my variables, went to ILLEGAL ISR and rebooted. Now it does not, but I'm not sure what I've changed.
So, I really don't know what to think. I'll try board with 28335 on next Monday. Can such problems be caused by bad contact in supply connectors? Maybe i should try changing emulator freq? I'm using SAU510 USB ISO. The lot trace code of DSP's is CA-8AAFJXW.