This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: I2C only writing last byte of buffer

Part Number: TMS320F28379D

First, I should note I've been able to succesfully run exampe code reading and writing to EEPROM (i2c_ex2_eeprom). Now, I am trying to write a contiguous stream of bytes larger than the 16 Byte FIFO. I've disabled the FIFO and tried two different methods.

  1. Repeat mode sending a start condition, then i2c_putData() to put my high address, low address, and data bytes then a stop condtion and waiting for XRDY to be 1 before each next byte.
  2. Non-repeat mode similiar to above but I set the number of bytes to write

Neither works. It will only ever write the last byte to the bus. On my scope it looks as follows:

  1. Repeat mode, Start Condition, Address, Last Byte, Stop condition
  2. Non-repeat mode, Start Condition, Address, Last Byte, NO Stop condition

SCLK is also stuck low if that helps. I've attached my code below. There's not much modification from the example. Is there a better way to write to EEPROM? None of the other posts seem to really solve my problem.

//#############################################################################
//
// FILE:   i2c_ex2_eeprom.c
//
// TITLE:  I2C EEPROM
//
//! \addtogroup driver_example_list
//! <h1>I2C EEPROM</h1>
//!
//! This program will write 1-14 words to EEPROM and read them back. The data
//! written and the EEPROM address written to are contained in the message
//! structure, i2cMsgOut. The data read back will be contained in the message
//! structure i2cMsgIn.
//!
//! \b External \b Connections \n
//!  - Connect external I2C EEPROM at address 0x50
//!  - Connect GPIO32/SDAA to external EEPROM SDA (serial data) pin
//!  - Connect GPIO33/SCLA to external EEPROM SCL (serial clock) pin
//!
//! \b Watch \b Variables \n
//!  - \b i2cMsgOut - Message containing data to write to EEPROM
//!  - \b i2cMsgIn - Message containing data read from EEPROM
//!
//
//#############################################################################
// $TI Release: F2837xD Support Library v3.07.00.00 $
// $Release Date: Sun Sep 29 07:34:54 CDT 2019 $
// $Copyright:
// Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################

//
// Included Files
//
#include "driverlib.h"
#include "device.h"

//
// Defines
//
#define SLAVE_ADDRESS               0x50
#define EEPROM_HIGH_ADDR            0x00
#define EEPROM_LOW_ADDR             0x30
#define NUM_BYTES                   28
#define MAX_BUFFER_SIZE             28      // Max is currently 14 because of
                                            // 2 address bytes and the 16-byte 
                                            // FIFO

//
// I2C message states for I2CMsg struct
//
#define MSG_STATUS_INACTIVE         0x0000 // Message not in use, do not send
#define MSG_STATUS_SEND_WITHSTOP    0x0010 // Send message with stop bit
#define MSG_STATUS_WRITE_BUSY       0x0011 // Message sent, wait for stop
#define MSG_STATUS_SEND_NOSTOP      0x0020 // Send message without stop bit
#define MSG_STATUS_SEND_NOSTOP_BUSY 0x0021 // Message sent, wait for ARDY
#define MSG_STATUS_RESTART          0x0022 // Ready to become master-receiver
#define MSG_STATUS_READ_BUSY        0x0023 // Wait for stop before reading data

//
// Error messages for read and write functions
//
#define ERROR_BUS_BUSY              0x1000
#define ERROR_STOP_NOT_READY        0x5555
#define SUCCESS                     0x0000

//
// Typedefs
//
struct I2CMsg 
{
    uint16_t msgStatus;                  // Word stating what state msg is in.
                                         // See MSG_STATUS_* defines above.
    uint16_t slaveAddr;                  // Slave address tied to the message.
    uint16_t numBytes;                   // Number of valid bytes in message.
    uint16_t memoryHighAddr;             // EEPROM address of data associated
                                         // with message (high byte).
    uint16_t memoryLowAddr;              // EEPROM address of data associated
                                         // with message (low byte).
    uint16_t msgBuffer[MAX_BUFFER_SIZE]; // Array holding message data.
};

//
// Globals
//
struct I2CMsg i2cMsgOut = {MSG_STATUS_SEND_WITHSTOP,
                           SLAVE_ADDRESS,
                           NUM_BYTES,
                           EEPROM_HIGH_ADDR,
                           EEPROM_LOW_ADDR,
                           0x01,                // Message bytes
                           0x23,
                           0x45,
                           0x67,
                           0x89,
                           0xAB,
                           0xCD,
                           0xEF,
                           0x12,                // Message bytes
                           0x34,
                           0x56,
                           0x78,
                           0x9A,
                           0xBC,
                           0xDE,
                           0xFF,
                           0xED,
                           0xCB,
                           0xA9,
                           0x87,
                           0x65,
                           0x43,
                           0x21,
                           0x00,
                           0xFF,
                           0xFF,
                           0xFF,
                           0xFF};
struct I2CMsg i2cMsgIn  = {MSG_STATUS_SEND_NOSTOP,
                           SLAVE_ADDRESS,
                           NUM_BYTES,
                           EEPROM_HIGH_ADDR,
                           EEPROM_LOW_ADDR};

struct I2CMsg *currentMsgPtr;                   // Used in interrupt

uint16_t passCount = 0;
uint16_t failCount = 0;

//
// Function Prototypes
//
void initI2C(void);
uint16_t readData(struct I2CMsg *msg);
uint16_t writeData(struct I2CMsg *msg);

void fail(void);
void pass(void);

__interrupt void i2cBISR(void);

//
// Main
//
void main(void)
{
    uint16_t error;
    uint16_t i;

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Disable pin locks and enable internal pullups.
    //
    Device_initGPIO();

    //
    // Initialize GPIOs 32 and 33 for use as SDA A and SCL A respectively
    //
    GPIO_setPinConfig(GPIO_40_SDAB);
    GPIO_setPadConfig(40, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(40, GPIO_QUAL_ASYNC);

    GPIO_setPinConfig(GPIO_41_SCLB);
    GPIO_setPadConfig(41, GPIO_PIN_TYPE_PULLUP);
    GPIO_setQualificationMode(41, GPIO_QUAL_ASYNC);

    //
    // Initialize PIE and clear PIE registers. Disable CPU interrupts.
    //
    Interrupt_initModule();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    //
    Interrupt_initVectorTable();

    //
    // Interrupts that are used in this example are re-mapped to ISR functions
    // found within this file.
    //
    Interrupt_register(INT_I2CB, &i2cBISR);

    //
    // Set I2C use, initializing it for FIFO mode
    //
    initI2C();

    //
    // Clear incoming message buffer
    //
    for (i = 0; i < MAX_BUFFER_SIZE; i++)
    {
        i2cMsgIn.msgBuffer[i] = 0x0000;
    }

    //
    // Set message pointer used in interrupt to point to outgoing message
    //
    currentMsgPtr = &i2cMsgOut;

    //
    // Enable interrupts required for this example
    //
    Interrupt_enable(INT_I2CB);

    //
    // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
    //
    EINT;
    ERTM;

    //
    // Loop indefinitely
    //
    while(1)
    {
        //
        // **** Write data to EEPROM section ****
        //
        // Check the outgoing message to see if it should be sent. In this
        // example it is initialized to send with a stop bit.
        //
        if(i2cMsgOut.msgStatus == MSG_STATUS_SEND_WITHSTOP)
        {
            //
            // Send the data to the EEPROM
            //
            error = writeData(&i2cMsgOut);

            //
            // If communication is correctly initiated, set msg status to busy
            // and update currentMsgPtr for the interrupt service routine.
            // Otherwise, do nothing and try again next loop. Once message is
            // initiated, the I2C interrupts will handle the rest. See the
            // function i2cAISR().
            //
            if(error == SUCCESS)
            {
                currentMsgPtr = &i2cMsgOut;
                i2cMsgOut.msgStatus = MSG_STATUS_WRITE_BUSY;
            }
        }

        //
        // **** Read data from EEPROM section ****
        //
        // Check outgoing message status. Bypass read section if status is
        // not inactive.
        //
        if (i2cMsgOut.msgStatus == MSG_STATUS_INACTIVE)
        {
            //
            // Check incoming message status
            //
            if(i2cMsgIn.msgStatus == MSG_STATUS_SEND_NOSTOP)
            {
                //
                // Send EEPROM address setup
                //
                while(readData(&i2cMsgIn) != SUCCESS)
                {
                    //
                    // Maybe setup an attempt counter to break an infinite
                    // while loop. The EEPROM will send back a NACK while it is
                    // performing a write operation. Even though the write
                    // is complete at this point, the EEPROM could still be
                    // busy programming the data. Therefore, multiple
                    // attempts are necessary.
                    //
                }

                //
                // Update current message pointer and message status
                //
                currentMsgPtr = &i2cMsgIn;
                i2cMsgIn.msgStatus = MSG_STATUS_SEND_NOSTOP_BUSY;
           }

            //
            // Once message has progressed past setting up the internal address
            // of the EEPROM, send a restart to read the data bytes from the
            // EEPROM. Complete the communique with a stop bit. msgStatus is
            // updated in the interrupt service routine.
            //
            else if(i2cMsgIn.msgStatus == MSG_STATUS_RESTART)
            {
                //
                // Read data portion
                //
                while(readData(&i2cMsgIn) != SUCCESS)
                {
                    //
                    // Maybe setup an attempt counter to break an infinite
                    // while loop.
                    //
                }

                //
                // Update current message pointer and message status
                //
                currentMsgPtr = &i2cMsgIn;
                i2cMsgIn.msgStatus = MSG_STATUS_READ_BUSY;
            }
        }
    }
}

//
// initI2C - Function to configure I2C A in FIFO mode.
//
void
initI2C()
{
    //
    // Must put I2C into reset before configuring it
    //
    I2C_disableModule(I2CB_BASE);

    //
    // I2C configuration. Use a 400kHz I2CCLK with a 33% duty cycle.
    //
    I2C_initMaster(I2CB_BASE, DEVICE_SYSCLK_FREQ, 400000, I2C_DUTYCYCLE_33);
    I2C_setBitCount(I2CB_BASE, I2C_BITCOUNT_8);
    I2C_setSlaveAddress(I2CB_BASE, SLAVE_ADDRESS);
    I2C_setEmulationMode(I2CB_BASE, I2C_EMULATION_FREE_RUN);

    //
    // Enable stop condition and register-access-ready interrupts
    //
    I2C_enableInterrupt(I2CB_BASE, I2C_INT_STOP_CONDITION |
                        I2C_INT_REG_ACCESS_RDY);

    //
    // FIFO configuration
    //
    //I2C_enableFIFO(I2CB_BASE);
    I2C_clearInterruptStatus(I2CB_BASE, I2C_INT_STOP_CONDITION);

    //
    // Configuration complete. Enable the module.
    //
    I2C_enableModule(I2CB_BASE);
}

//
// writeData - Function to send the data that is to be written to the EEPROM
//
uint16_t
writeData(struct I2CMsg *msg)
{
    uint16_t i;

    //
    // Wait until the STP bit is cleared from any previous master
    // communication. Clearing of this bit by the module is delayed until after
    // the SCD bit is set. If this bit is not checked prior to initiating a new
    // message, the I2C could get confused.
    //
    if(I2C_getStopConditionStatus(I2CB_BASE))
    {
        return(ERROR_STOP_NOT_READY);
    }
    I2C_setConfig(I2CB_BASE, I2C_MASTER_SEND_MODE | I2C_REPEAT_MODE);
    //
    // Setup slave address
    //
    I2C_setSlaveAddress(I2CB_BASE, SLAVE_ADDRESS);

    //
    // Check if bus busy
    //
    if(I2C_isBusBusy(I2CB_BASE))
    {
        return(ERROR_BUS_BUSY);
    }

    //
    // Setup number of bytes to send msgBuffer and address
    //
    I2C_setDataCount(I2CB_BASE, (msg->numBytes + 2));

    I2C_sendStartCondition(I2CB_BASE);
    //I2C_sendStopCondition(I2CB_BASE);
    //
    // Setup data to send
    //
    while(I2C_getStatus(I2CB_BASE) & I2C_STS_TX_DATA_RDY == 0);
    I2C_putData(I2CB_BASE, msg->memoryHighAddr);
    while(I2C_getStatus(I2CB_BASE) & I2C_STS_TX_DATA_RDY == 0);
    I2C_putData(I2CB_BASE, msg->memoryLowAddr);

    for (i = 0; i < msg->numBytes; i++)
    {
        while(I2C_getStatus(I2CB_BASE) & I2C_STS_TX_DATA_RDY == 0);
        I2C_putData(I2CB_BASE, msg->msgBuffer[i]);
    }

    //
    // Send start as master transmitter
    //
    //I2C_setConfig(I2CB_BASE, I2C_MASTER_SEND_MODE);
    //I2C_sendStartCondition(I2CB_BASE);
    I2C_sendStopCondition(I2CB_BASE);

    return(SUCCESS);
}

//
// readData - Function to prepare for the data that is to be read from the EEPROM
//
uint16_t
readData(struct I2CMsg *msg)
{
    //
    // Wait until the STP bit is cleared from any previous master
    // communication. Clearing of this bit by the module is delayed until after
    // the SCD bit is set. If this bit is not checked prior to initiating a new
    // message, the I2C could get confused.
    //
    if(I2C_getStopConditionStatus(I2CB_BASE))
    {
        return(ERROR_STOP_NOT_READY);
    }

    //
    // Setup slave address
    //
    I2C_setSlaveAddress(I2CB_BASE, SLAVE_ADDRESS);

    //
    // If we are in the the address setup phase, send the address without a
    // stop condition.
    //
    if(msg->msgStatus == MSG_STATUS_SEND_NOSTOP)
    {
        //
        // Check if bus busy
        //
        if(I2C_isBusBusy(I2CB_BASE))
        {
            return(ERROR_BUS_BUSY);
        }

        //
        // Send data to setup EEPROM address
        //
        I2C_setDataCount(I2CB_BASE, 2);
        I2C_putData(I2CB_BASE, msg->memoryHighAddr);
        I2C_putData(I2CB_BASE, msg->memoryLowAddr);
        I2C_setConfig(I2CB_BASE, I2C_MASTER_SEND_MODE);
        I2C_sendStartCondition(I2CB_BASE);
    }
    else if(msg->msgStatus == MSG_STATUS_RESTART)
    {
        //
        // Address setup phase has completed. Now setup how many bytes expected
        // and send restart as master-receiver.
        //
        I2C_setDataCount(I2CB_BASE, (msg->numBytes));
        I2C_setConfig(I2CB_BASE, I2C_MASTER_RECEIVE_MODE);
        I2C_sendStartCondition(I2CB_BASE);
        I2C_sendStopCondition(I2CB_BASE);
    }

    return(SUCCESS);
}

//
// i2cAISR - I2C A ISR (non-FIFO)
//
__interrupt void
i2cBISR(void)
{
    I2C_InterruptSource intSource;
    uint16_t i;

    //
    // Read interrupt source
    //
    intSource = I2C_getInterruptSource(I2CB_BASE);

    //
    // Interrupt source = stop condition detected
    //
    if(intSource == I2C_INTSRC_STOP_CONDITION)
    {
        //
        // If completed message was writing data, reset msg to inactive state
        //
        if(currentMsgPtr->msgStatus == MSG_STATUS_WRITE_BUSY)
        {
            currentMsgPtr->msgStatus = MSG_STATUS_INACTIVE;
        }
        else
        {
            //
            // If a message receives a NACK during the address setup portion of
            // the EEPROM read, the code further below included in the register
            // access ready interrupt source code will generate a stop
            // condition. After the stop condition is received (here), set the
            // message status to try again. User may want to limit the number
            // of retries before generating an error.
            //
            if(currentMsgPtr->msgStatus == MSG_STATUS_SEND_NOSTOP_BUSY)
            {
                currentMsgPtr->msgStatus = MSG_STATUS_SEND_NOSTOP;
            }
            //
            // If completed message was reading EEPROM data, reset message to
            // inactive state and read data from FIFO.
            //
            else if(currentMsgPtr->msgStatus == MSG_STATUS_READ_BUSY)
            {
                currentMsgPtr->msgStatus = MSG_STATUS_INACTIVE;
                for(i=0; i < NUM_BYTES; i++)
                {
                    currentMsgPtr->msgBuffer[i] = I2C_getData(I2CB_BASE);
                }

                //
                // Check received data
                //
                for(i=0; i < NUM_BYTES; i++)
                {
                    if(i2cMsgIn.msgBuffer[i] == i2cMsgOut.msgBuffer[i])
                    {
                        passCount++;
                    }
                    else
                    {
                        failCount++;
                    }
                }

                if(passCount == NUM_BYTES)
                {
                    pass();
                }
                else
                {
                    fail();
                }
            }
        }
    }
    //
    // Interrupt source = Register Access Ready
    //
    // This interrupt is used to determine when the EEPROM address setup
    // portion of the read data communication is complete. Since no stop bit
    // is commanded, this flag tells us when the message has been sent
    // instead of the SCD flag.
    //
    else if(intSource == I2C_INTSRC_REG_ACCESS_RDY)
    {
        //
        // If a NACK is received, clear the NACK bit and command a stop.
        // Otherwise, move on to the read data portion of the communication.
        //
        if((I2C_getStatus(I2CB_BASE) & I2C_STS_NO_ACK) != 0)
        {
            I2C_sendStopCondition(I2CB_BASE);
            I2C_clearStatus(I2CB_BASE, I2C_STS_NO_ACK);
        }
        else if(currentMsgPtr->msgStatus == MSG_STATUS_SEND_NOSTOP_BUSY)
        {
            currentMsgPtr->msgStatus = MSG_STATUS_RESTART;
        }
    }
    else
    {
        //
        // Generate some error from invalid interrupt source
        //
        asm("   ESTOP0");
    }

    //
    // Issue ACK to enable future group 8 interrupts
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
}

//
// pass - Function to be called if data written matches data read
//
void
pass(void)
{
    asm("   ESTOP0");
    for(;;);
}

//
// fail - Function to be called if data written does NOT match data read
//
void fail(void)
{
    asm("   ESTOP0");
    for(;;);
}

//
// End of File
//

  • So, in thinking about this more, I began to run some experiments. It felt like the data written to I2CDXR was getting clobbered, even though I was checking XRDY to be set. It was also feeling like even though I'm waiting for the XRDY bit to be set, maybe it was always set. Meaning it never clears when I write data to I2CDXR. When stepping through with the debugger it never seems to clear. Perhaps it happens too fast for the IDE to catch it in the Registers window. Not sure.

    I have found, however, if I insert a slight delay before I put a new byte into I2CDXR it in fact works as expected. A work around, sure, but I still want to know if I'm actually misunderstanding how these registers and status bits work, since the idea of inserting an aribtrary delay doesn't feel like the best solution.

  • Geoffrey,

    It is true that XRDY bit is in cleared state only for a short time.

    Can you please let us know where you had to add the additional delay? And how much delay did you have to add?

    Regards,

    Manoj

  • Below is the code I'm using to get it to run successfully. I've poked around in registers all day. I've set breakpoints immediately after the write. The XRDY bit never clears so it immediately wants to write the next byte to the register.I've used SysCtl_delay(1000) to insert the delay before every single byte I write. Anything significantly less than 1000 cycles and I start to get undefined behavior where it may not write all of the bytes. On a 200MHz processor, a delay of 1000 cycles should be equivalent to ~5us. Below I've attached the modified writeData() function.

    #define DELAY 1000
    
    //
    // writeData - Function to send the data that is to be written to the EEPROM
    //
    uint16_t
    writeData(struct I2CMsg *msg)
    {
        uint16_t i, status;
    
        //
        // Wait until the STP bit is cleared from any previous master
        // communication. Clearing of this bit by the module is delayed until after
        // the SCD bit is set. If this bit is not checked prior to initiating a new
        // message, the I2C could get confused.
        //
        if(I2C_getStopConditionStatus(I2CB_BASE))
        {
            return(ERROR_STOP_NOT_READY);
        }
        I2C_setConfig(I2CB_BASE, I2C_MASTER_SEND_MODE);
        //
        // Setup slave address
        //
        I2C_setSlaveAddress(I2CB_BASE, SLAVE_ADDRESS);
    
        //
        // Check if bus busy
        //
        if(I2C_isBusBusy(I2CB_BASE))
        {
            return(ERROR_BUS_BUSY);
        }
    
        //
        // Setup number of bytes to send msgBuffer and address
        //
        I2C_setDataCount(I2CB_BASE, (msg->numBytes + 2));
    
        I2C_sendStartCondition(I2CB_BASE);
        I2C_sendStopCondition(I2CB_BASE);
        //
        // Setup data to send
        //
        while(I2C_getStatus(I2CB_BASE) & I2C_STS_TX_DATA_RDY == 0);
        SysCtl_delay(DELAY);
        I2C_putData(I2CB_BASE, msg->memoryHighAddr);
    
        while(I2C_getStatus(I2CB_BASE) & I2C_STS_TX_DATA_RDY == 0);
        SysCtl_delay(DELAY);
        I2C_putData(I2CB_BASE, msg->memoryLowAddr);
    
        for (i = 0; i < msg->numBytes; i++)
        {
            while(I2C_getStatus(I2CB_BASE) & I2C_STS_TX_DATA_RDY == 0);
            SysCtl_delay(DELAY);
            I2C_putData(I2CB_BASE, msg->msgBuffer[i]);
        }
    
        //
        // Send start as master transmitter
        //
        //I2C_setConfig(I2CB_BASE, I2C_MASTER_SEND_MODE);
        //I2C_sendStartCondition(I2CB_BASE);
        //I2C_sendStopCondition(I2CB_BASE);
    
        return(SUCCESS);
    }