Other Parts Discussed in Thread: UNIFLASH
Hi Guys, just a quick question. I'm using the TI ControlCARD Docking station [R4.1] with my 28377D control card [R1.1] to experiment with, which works great BTW. I totally LOVE C2000 Assembler. :)
Anyway, I'll be designing my own 176 PIN 28377D standalone board and I was wondering if you can help with what I would need, like what software I would need to download my assembly code and which flash programmer I would need to use. I'm reading up on downloading the code to a standalone board and the communication mode it uses is the SCI USART mode which seems pretty easy to use but I'm not sure what I would need to do to that. lol. Any pointers would be muchly appreciated.
Thanks guys and hope to hear from you soon.
Pete