This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: TMS320F28335

Part Number: TMS320F28335
Other Parts Discussed in Thread: TMDSDOCK28335

Tool/software: Code Composer Studio

What are the Main Difference for Both below Boards,

TMDSPREX28335 and TMDSDOCK28335  are the two versions of the boards. .....?

  • Kameshwaran,

    Both are good evaluation platforms. They both work for evaluating an F2833x device.

    TMDSDOCK28335 

    • Basic evaluation platform for F2833x devices
    • Contains an F28335 and everything you need to set it up and run code
    • Breaks out many device pins

    TMDSPREX28335

    • Contains an F28335 and everything you need to set it up and run code
    • Breaks out some device pins
    • Contains lots of hardware to show off realistic use cases for the peripherals on an F2833x device

    If you just want to debug and run code or develop and test your own hardware TMDSDOCK28335 is best. If you're looking to learn about an F2833x device, and want some external hardware to interact with, but you do not want to build or customize the hardware then TMDSPREX28335 is best.

    TMDSDOCK28335 will get you going and prototyping, TMDSPREX28335 will get you going and learning with external hardware without the need to prototype any hardware.

    Regards,
    Cody 

  • Thanks Cody,

    Thanks For  the  Clarify My Queries....

    I am clearly understand about that topic.....!