Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Hello,
I am trying to program the ePWM Trip Zone using a LAUNCHXL-F28379D development board. I would like to set a GPIO pin to trip the PWM outputs in case of a fault. I have set the GPIO32 pin to input and set it to feed TZ1 using Xbar. I have also enables the TZSEL.bit.OSHT1 as a one shot trip source to just trip the converter until resetting. TZCTL.bit.TZA was set to force low. However applying a High (3.3V) to input pin GPIO32 is not stopping the PWM output. I must have missed something. Can someone kindly offer some help, please?
Thanks