Part Number: F28M36P63C2
Dear all,
I have two inverters that work well in stand-alone mode and i want now to operate them in parallel. All the control part is implemented in the Simulink add-on for concerto microcontrollers. The microcontroller i am using is the F28M36P63C2.
The problem i am facing is as follows: when i start operating one of the inverters (inverter 1) with the load and then i want to synchronize the second inverter ( inverter 2), inverter 2 needs to read the voltage at the connection point without connecting (i.e. without closing the relays). Even though at the output of voltage sensor of the 2nd inverter, the waveform is very good, in the CCS graph, every 10-15s this voltage gets very noisy for some seconds and then returns to normal. Thus, it is not safe to try connect.
Maybe the problem is related to the fact that i use the ePWM ADC SOCA for triggering the ADC inputs. Note that when the relays are open, the PWM signals of the second inverter do not correspond to the connection point voltage, which i am trying to read (the pwm signals of the second inverter are not those that create the connection/load voltage i am trying to read, which is created by inverter 1). I am not sure if this exactly is the problem or how i should proceed.
Has anyone faced anything similar before? Any hint would be very helpful.
Thanks in advance.
Alex