Other Parts Discussed in Thread: MAX232
Hi Vamsi, thanks for the info.
For serial programming and interfacing to my standalone board would I have to connect the PC's TX line to a MAX232 and from the MAX232 to the F28377D's RX line and connect the PC's RX line to the TX line of the MAX232 and the F2837D's TX line to the MAX232 RX line?
Or can I connect the PC's TX and RX lines directly to the F28377D's RX and TX lines? The reason I ask this is I don't know if the F28377D's RX and TX lines are 5volt tolerant. If I remember correctly the PC's serial ports run at 5Volts. I could be wrong but its better to ask to be sure.
Please let me know your thoughts.
Thanks again for your help.
Peter