Hi
I have a F2837x project that sets PWM1 and PWM2 as high resolution PWMs.
At the very beginning the program calls HRPwmCalibration() function and when
it enters SFO() it doesn't return from the function.
I have checked TI's high resolution PWM example and couldn't find any clue.
I have uploaded the project as below.
It also can be reached at the link below:
www.powersimtech.com/.../TestPhaseShift1.zip
thanks,
Jiakai