Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Question about Cla1ForceTask1andWait()

Genius 3095 points

Part Number: TMS320F28377D

Dear team:

When use TI's routine  and run in RAM, the CLA can run normally.

Now I migrate part of the cla program to my own project, and initialize some parameters in the CLA task, Program will stuck in cla1forcetask1andwait() and waiting for task 1 to complete. Here is part of my code, What improvements can I make?

// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C



MEMORY
{
PAGE 0 :
   /* BEGIN is used for the "boot to SARAM" bootloader mode   */

   BEGIN            : origin = 0x080000, length = 0x000002
   RAMM0            : origin = 0x000080, length = 0x000380
   RAMD0            : origin = 0x00B000, length = 0x000800
   RAMLS0           : origin = 0x008000, length = 0x000800

   RAMLS2           : origin = 0x009000, length = 0x000800
   RAMLS3           : origin = 0x009800, length = 0x000800
   RAMLS4           : origin = 0x00A000, length = 0x000800
   RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS15          : origin = 0x01B000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RESET            : origin = 0x3FFFC0, length = 0x000002

   /* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE  /* on-chip Flash */
   FLASHB           : origin = 0x082000, length = 0x002000  /* on-chip Flash */
   FLASHC           : origin = 0x084000, length = 0x002000  /* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000  /* on-chip Flash */
   FLASHE           : origin = 0x088000, length = 0x008000  /* on-chip Flash */
   FLASHF           : origin = 0x090000, length = 0x008000  /* on-chip Flash */
   FLASHG           : origin = 0x098000, length = 0x008000  /* on-chip Flash */
   FLASHH           : origin = 0x0A0000, length = 0x008000  /* on-chip Flash */
   FLASHI           : origin = 0x0A8000, length = 0x008000  /* on-chip Flash */
   FLASHJ           : origin = 0x0B0000, length = 0x008000  /* on-chip Flash */
   FLASHK           : origin = 0x0B8000, length = 0x002000  /* on-chip Flash */
   FLASHL           : origin = 0x0BA000, length = 0x002000  /* on-chip Flash */
   FLASHM           : origin = 0x0BC000, length = 0x002000  /* on-chip Flash */
   FLASHN           : origin = 0x0BE000, length = 0x002000  /* on-chip Flash */

PAGE 1 :

   BOOT_RSVD       : origin = 0x000002, length = 0x00007E     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMD1           : origin = 0x00B800, length = 0x000800

   RAMLS1           : origin = 0x008800, length = 0x000800
   RAMLS5          : origin = 0x00A800, length = 0x000800


   RAMGS0      : origin = 0x00C000, length = 0x001000
   RAMGS1      : origin = 0x00D000, length = 0x001000
   RAMGS2      : origin = 0x00E000, length = 0x001000
   RAMGS3      : origin = 0x00F000, length = 0x001000
   RAMGS4      : origin = 0x010000, length = 0x001000
   RAMGS5      : origin = 0x011000, length = 0x001000
   RAMGS6      : origin = 0x012000, length = 0x001000
   RAMGS7      : origin = 0x013000, length = 0x001000
   RAMGS8      : origin = 0x014000, length = 0x001000
   RAMGS9      : origin = 0x015000, length = 0x001000
   RAMGS10     : origin = 0x016000, length = 0x001000
   RAMGS11     : origin = 0x017000, length = 0x001000
   RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */


   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400

   CLA1_MSGRAMLOW   : origin = 0x001480,   length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500,   length = 0x000080
}

SECTIONS
{
   /* Allocate program areas: */
   .cinit              : > FLASHE      PAGE = 0, ALIGN(8)
   .text               : >> FLASHE | FLASHF | FLASHG      PAGE = 0, ALIGN(8)
   codestart           : > BEGIN       PAGE = 0, ALIGN(8)

   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1        PAGE = 1

   /* Initalized sections go in Flash */
   .switch             : > FLASHE      PAGE = 0, ALIGN(8)
   .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
   

   .pinit              : > FLASHE,       PAGE = 0,       ALIGN(8)
   .ebss               : >> RAMLS5 | RAMGS10 | RAMGS11,    PAGE = 1
   .esysmem            : > RAMLS5,       PAGE = 1
   .cio                : > RAMLS5,       PAGE = 1
   /* Initalized sections go in Flash */
   .econst             : > FLASHE       PAGE = 0, ALIGN(8)


   CLADataLS1       : > RAMLS1, PAGE=1


   Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW,   PAGE = 1
   CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH,  PAGE = 1


   CPU01_SHARE_RAM    : > RAMGS0,    PAGE = 1  /*CPU01数据区*/
   CPU02_SHARE_RAM    : > RAMGS1,    PAGE = 1  /*CPU02数据区*/

#ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000
        #if defined(__TI_EABI__)
            .TI.ramfunc : {} LOAD = FLASHE,
                                 RUN = RAMLS0,
                                 LOAD_START(RamfuncsLoadStart),
                                 LOAD_SIZE(RamfuncsLoadSize),
                                 LOAD_END(RamfuncsLoadEnd),
                                 RUN_START(RamfuncsRunStart),
                                 RUN_SIZE(RamfuncsRunSize),
                                 RUN_END(RamfuncsRunEnd),
                                 PAGE = 0, ALIGN(8)
        #else
            .TI.ramfunc : {} LOAD = FLASHE,
                             RUN = RAMLS0,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_SIZE(_RamfuncsLoadSize),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             RUN_SIZE(_RamfuncsRunSize),
                             RUN_END(_RamfuncsRunEnd),
                             PAGE = 0, ALIGN(8)
        #endif
    #else
   ramfuncs            : LOAD = FLASHE,
                         RUN = RAMLS0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(8)
    #endif
#endif

    /* CLA specific sections */
   #if defined(__TI_EABI__)
        Cla1Prog    : LOAD = FLASHE,
                      RUN = RAMLS4,
                      LOAD_START(Cla1funcsLoadStart),
                      LOAD_END(Cla1funcsLoadEnd),
                      RUN_START(Cla1funcsRunStart),
                      LOAD_SIZE(Cla1funcsLoadSize),
                      PAGE = 0, ALIGN(8)
   #else
        Cla1Prog    : LOAD = FLASHE,
                      RUN = RAMLS4,
                      LOAD_START(_Cla1funcsLoadStart),
                      LOAD_END(_Cla1funcsLoadEnd),
                      RUN_START(_Cla1funcsRunStart),
                      LOAD_SIZE(_Cla1funcsLoadSize),
                      PAGE = 0, ALIGN(8)
   #endif



   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }

    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }


    #ifdef CLA_C
   /* CLA C compiler sections */
   //
   // Must be allocated to memory the CLA has write access to
   //
   CLAscratch       :
                     { *.obj(CLAscratch)
                     . += CLA_SCRATCHPAD_SIZE;
                     *.obj(CLAscratch_end) } >  RAMLS2,  PAGE = 0

   .scratchpad      : > RAMLS2,       PAGE = 0
   .bss_cla         : > RAMLS2,       PAGE = 0
   .const_cla       :  LOAD = FLASHE,
                       RUN = RAMLS2,
                       RUN_START(_Cla1ConstRunStart),
                       LOAD_START(_Cla1ConstLoadStart),
                       LOAD_SIZE(_Cla1ConstLoadSize),
                       PAGE = 0
#endif //CLA_C

}

/*
//===========================================================================
// End of file.
//===========================================================================
//
// CLA_configClaMemory - Configure CLA memory sections
//
void CLA_configClaMemory(void)
{
    extern uint32_t Cla1funcsRunStart, Cla1funcsLoadStart, Cla1funcsLoadSize;
    EALLOW;

#ifdef _FLASH
    //
    // Copy over code from FLASH to RAM
    //
    memcpy((uint32_t *)&Cla1funcsRunStart, (uint32_t *)&Cla1funcsLoadStart,
            (uint32_t)&Cla1funcsLoadSize);
#endif //_FLASH

    //
    // Initialize and wait for CLA1ToCPUMsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CLA1TOCPU = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CLA1TOCPU != 1){};

    //
    // Initialize and wait for CPUToCLA1MsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CPUTOCLA1 = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CPUTOCLA1 != 1){};

    //
    // Select LS4RAM and LS5RAM to be the programming space for the CLA
    // First configure the CLA to be the master for LS4 and LS5 and then
    // set the space to be a program block
    //
    MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;

    //
    // Next configure LS0RAM and LS1RAM as data spaces for the CLA
    // First configure the CLA to be the master for LS0(1) and then
    // set the spaces to be code blocks
    //

    MemCfgRegs.LSxMSEL.bit.MSEL_LS1 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS1 = 0;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS2 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS2 = 0;



    EDIS;
}


//
// CLA_initCpu2Cla1 -  Initialize CLA task vectors and end of task interrupts
//
void CLA_initCpu2Cla1(void)
{
    //
    // Compute all CLA task vectors
    // On Type-1 CLAs the MVECT registers accept full 16-bit task addresses as
    // opposed to offsets used on older Type-0 CLAs
    //
    EALLOW;
    Cla1Regs.MVECT1 = (uint16_t)(&Cla1Task1);
    Cla1Regs.MVECT2 = (uint16_t)(&Cla1Task2);
    Cla1Regs.MVECT3 = (uint16_t)(&Cla1Task3);
    Cla1Regs.MVECT4 = (uint16_t)(&Cla1Task4);
    Cla1Regs.MVECT5 = (uint16_t)(&Cla1Task5);
    Cla1Regs.MVECT6 = (uint16_t)(&Cla1Task6);
    Cla1Regs.MVECT7 = (uint16_t)(&Cla1Task7);
    Cla1Regs.MVECT8 = (uint16_t)(&Cla1Task8);

    //
    // Enable the IACK instruction to start a task on CLA in software
    // for all  8 CLA tasks. Also, globally enable all 8 tasks (or a
    // subset of tasks) by writing to their respective bits in the
    // MIER register
    //
    Cla1Regs.MCTL.bit.IACKE = 1;
    Cla1Regs.MIER.all = 0x00FF;

    //
    // Configure the vectors for the end-of-task interrupt for all
    // 8 tasks
    //
    PieVectTable.CLA1_1_INT = &cla1Isr1;
    PieVectTable.CLA1_2_INT = &cla1Isr2;
    PieVectTable.CLA1_3_INT = &cla1Isr3;
    PieVectTable.CLA1_4_INT = &cla1Isr4;
    PieVectTable.CLA1_5_INT = &cla1Isr5;
    PieVectTable.CLA1_6_INT = &cla1Isr6;
    PieVectTable.CLA1_7_INT = &cla1Isr7;
    PieVectTable.CLA1_8_INT = &cla1Isr8;

    //
    // Set the adcB.1 as the trigger for task 2
    //
    DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = 0;
    DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK2 = 6;

    //
    // Enable CLA interrupts at the group and subgroup levels
    //
    PieCtrlRegs.PIEIER11.all = 0xFFFF;
    IER |= (M_INT11 );
}
void main(void)
{
 Uint16 led_flag=0;

   InitSysCtrl();

#ifdef _FLASH
   InitFlash();
#endif

    DINT;

    InitPieCtrl();

    IER = 0x0000;
    IFR = 0x0000;

    InitPieVectTable();

    //初始化CLA
    CLA_configClaMemory();
    CLA_initCpu2Cla1();

    //使能需要 IER中断
    IER |= M_INT1;
    IER |= M_INT10;

    //开启 pie 中断使能
 //   PieCtrlRegs.PIEIER1.bit.INTx7 = 1; //定时器

    EINT;  // Enable Global interrupt INTM
    ERTM;  // Enable Global realtime interrupt DBGM

    //CLA参数初始化
 <span style="background-color:#ff0000;">  Cla1ForceTask1andWait();</span>

//    AdcaRegs.ADCSOCFRC1.all = 0x3F;
//    AdcbRegs.ADCSOCFRC1.all = 0x1E;
//    AdccRegs.ADCSOCFRC1.all = 0x0E;
//    AdcdRegs.ADCSOCFRC1.all = 0x3F;

    for(;;)
    {
    }
}

Best regards