This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 eCAN ; TSEG2REG = 0 error



Hi,

I'm using  the eCan in the 28335.

This may be a user IQ issue but I do not see why I cannot set TSEG2REG = 0, however this causes the CANES.bit.CCE bit to never be cleared. I can set TSEG2REG = 1 and it clears.

Which part of the manual have I not read correctly? BRPREG = 11 and TSEG1REG= 5 ?

Thanks.