Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE
Hi Nitin,
Have you checked the setting of WD register in CCS register view to make sure the configuration is as expected. Please note that WD registers are EALLOW protected so you need to use the EALLOW instruction before updating them. Please refer the WD example in C2000Ware for reference.
Regards,
Vivek Singh
So watchdog is always in disable state even though I'm enabling it forcefully.
Thanks & Regards,
Nitin K.
Nitin,
WdRegs.WDCR.all = 0 is not correct way to write this register. You need to write the WDCHK field as "101" to enable write to this register hence value you need to write is "28".
WdRegs.WDCR.all = 0x28;
Regards,
Vivek Singh
Vivek,
Writing "WdRegs.WDCR.all = 0x28" enables the watchdog.
I can see WDIS bit is = 0, after writing above instruction.
Now, I'm not resetting the watchdog counter anywhere in the code, so device should reset as soon as watchdog counter overflows.
I'm checking in the debug mode, as soon as watchdog counter overflows compiler shows error : "No source available for 0x3FB02A"
How can I confirm that unit is getting reset because of watchdog or it is getting stuck somewhere.
Thanks & Regards,
Nitin
Hi Nitin,
If you are getting "No source available for 0x3FB02A" message then it means device got reset and started executing BOOTROM code for which source code is not available. You can look into RESC register status to know what has caused the reset.
Regards,
Vivek Singh