Part Number: DRV8312-69M-KIT
Other Parts Discussed in Thread: C2000WARE
With respect to attached BLDC motor specs (DT4260-24-055-04H-PT make)., we have few questions for using right parameters for PID.
1. PID tends to go into saturation (pwm1.DutyFunc jumps to 31129) as soon as ILoopFlag is set & CurrentSet = 1.2. [to apply load, motor shaft is just held by hand]
2. The base quantities are chosen as below to initialize Kp:
BASE_VOLTAGE = 13.85 [24 / sqrt (3)]
BASE_CURRENT = 3.5 [Rated Torque / Torque Constant]
BASE_FREQ = 230
3. How to choose correct Umax & Umin for above configuration?
4 .Speed RPM goes seems to go into the range of 10000. Is it valid speed? How can we verify motor speed?