This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single conversion with adc - can't write register

Hi,

I want to get conversion with the adc, but I the flags at eoc were never set. I'm using the renewable enegery kit with an 28035 microcontroller.

Edit: I just checked, that none of the AdcRegs registers are written - But I tried to access the GPIO registers and it worked with this code expample in the same .c file

 

EALLOW;
                   GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 1;        
                   GpioCtrlRegs.GPBDIR.bit.GPIO34     = 1;

EDIS;

 

------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Here's my code

 

    watchdog(disable);                                // Watchdog: on/off

     init_adc();                                               // Power Up ADC

/***********************************
 * SOC0 CONFIG ****************
 * *********************************/
 
     EALLOW;
    AdcRegs.ADCSOC0CTL.bit.CHSEL     = Vdc;        // Input Voltage Vdc to Soc0 (ADCINA2)
     AdcRegs.ADCSOC0CTL.bit.ACQPS      = 6;         //set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
    AdcRegs.ADCSOC0CTL.bit.TRIGSEL     = 0;        // Softwaretrigger only
   
   
// Interrupt 1 forr SOC0
    AdcRegs.INTSEL1N2.bit.INT1E     = 1;                  // Enable Interrupt 1   
    AdcRegs.INTSEL1N2.bit.INT1CONT     = 0;          // no interupts till flag clear
    AdcRegs.ADCINTSOCSEL1.bit.SOC0     = 2;        // ADCINT2 triggers Soc0
   
/********************************************************************************************************/
 
// Interrupt 2 für EOC
    AdcRegs.INTSEL1N2.bit.INT2E                 = 1;                // Enable Interrupt 2
    AdcRegs.ADCCTL1.bit.INTPULSEPOS    = 1;    
    AdcRegs.INTSEL1N2.bit.INT2SEL            = 0;                // Connect ADCINT2 to EOC0
    AdcRegs.INTSEL1N2.bit.INT2CONT         = 0;         

    AdcRegs.ADCSOCFRC1.bit.SOC0     = 1;                      // Force start SOC0
    EDIS;       

Wether the AdcRegs.ADCSOCFLG1.bit.SOC0 nor the AdcRegs.ADCINTFLG.bit.ADCINT2 bit is set to one. Would be glad, if anyone can help me.