This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failed Software Reset F2812 CCS3.1

Dear,

I'm stuck on this problems. I can connect to ezdspF2812 easily, then load program (.out file) successful, but when reset (Ctrl+R), a error message displayed:

Failed Software Reset: Error 0x00000024/-1147 Error during: Register, Execution,  It appears that the target is being held in reset.  If this is a multi-core system, the master CPU may not be releasing the DSP from reset.  Please check your configuration in CCSetup and/or your GEL file to ensure that nothing is blocking the DSP from being released from reset.

Card worked fine in the past, nothing modify or changing hardware (ezdspTMS320F2812), so i dont know why i face this problem. I've googled and find many people face this too but i cant find any solution. Hope you can give me some diagnostics. Thank for pay attention!

Best regards,