Hi,
My design has two input signals - one is a synchronization digital input pulse and the second is an analog input being fed to the ADC.
When the synchronizing digital input makes a rising transition, I wish to take multiple (10-16) successive equi-distant/ equi-spaced samples of the the analog input channel.
Presently, one way to do is to have multiple SOCs (say 10), select the digital input as trigsel for each of them and have different ACQPS.
With a clock time period of 40ns and each SOC being successively 10 CC delayed - so SOC0 is after 10 CC from trigger, SOC1 is after 20 CC from trigger and so on, will the S+H timing for the ADC be met for each sample ?
If not, what is the recommended way to do it ?
Thanks and best regards
Bhawandeep Singh