Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: TMDSCNCD28035,
I am Using LANCHXL-F28069M and Altair Solid Thinking Embed(Model-Based Code generation Tool)
I have Destroyed(3.3V and Ground Short Circuited and Microcontroller is heating) totally Four LANCHXL-F28069M boards as of now.
After First Failure, I came to know that Board Cant tolerate 5V.
then after, three Boards also Destroyed. but I can't figure out the reason.
I got demotivated Because of the Continuos Failures and stopped Working in that area.
Now I wanna start Again but this time with F28035 control Card and Docking Station(TMDSCNCD28035).
1. What are the conditions that make 3.3V and Ground Short Circuited and Microcontroller is heating? How to avoid it?
2. What Are the precautions I should Take while Working With Controller boards?
eg : TMDSCNCD28035 and LAUNCHXL-F28069M
3. I am using older Laptops. Will there be any problem with the laptop USB ports?
4. What Kind of Environment I should work?
can some please help me.
Thanks In Advance