Part Number: TMS320F28377D-EP
Other Parts Discussed in Thread: TMS320F28377D
Tool/software: Code Composer Studio
Hi,
I am aware that in order to erase and program the flash on TMS320F28377D Launchpads, TI C2000 Device Support is required (version 4.2.5.0 or greater).
However, for my installation of CCS (8.1.0.00011) this is not installed. On trying to install it (Help -> Install New Software) it is noted that version 5.0.2.0 exists. But, the installation quits giving the following error,
An error occurred while collecting items to be installed
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No artifact repository available.
noArtifactRepositoriesAvailable
Updating CCS itself is not an option, as the version of the IDE has to be the same as the other developers working on the same project.