This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375S: Power Sequencing of VDDIO and VDDA

Part Number: TMS320F28375S


Hi,

In the controller datasheet (SPRS881G), section 5.9.1.2. It was given that "The 3.3-V supplies should be powered up together and kept within 0.3 V of each other during functional operation".

In our custom board, the supplies are generated from two different switcher IC's and there is a delay of 5mS between VDDA and VDDIO.

Although I'm not having any issue, will this cause a problem to the controller?

Regards

Kiran