This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301-69M-KIT: Parameter specification

Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM, LAUNCHXL-F28069M

Hello im looking for a PMSM motor controller. The motor i want to drive has some specific parameters in the pdf below. Where can i find the Datasheet of the microcontroller so i know that can drive this specific motor ID881 - RN 111-17 - WB 702 - 36V DC - OP without FW.PDF

  • yes, InstaSPIN-FOC should work well for this motor for torque/velocity control

    The DRV8301-69M-KIT EVM is probably the best kit for you to insure you have enough peak current, but it does have some drawbacks. The current sense is a little noisy and unbalanced.  It could be improved when you design your own board.

    Another option is using BOOSTXL-DRV8305EVM (15A Max) and LAUNCHXL-F28069M

    lower cost, better current sense, but maybe not quite enough power for full load tests.

  • Thank you btw i have a issue 

    i can't find the output constant and peak current and Volts in any of the relevant product. Is there not a datasheet that specifies this parameters

  • as an example on the BOOSTXL-DRV8305EVM page it states

    • 4.4V to 45V voltage supply input
    • Supports up to 20A peak, 15A continuous current ouput