Other Parts Discussed in Thread: DRV3201-Q1, CONTROLSUITE, MOTORWARE
Hi All,
I am working with BLDC - Block commutation control using DRV3201-Q1 and TMS320F28379D.
I am facing issue regarding DRV3201 that I can not turn off the both the GHSx and GLSx at the same time. As I am using block commutation i need to turn off gate (MOSFET) High and Low at same time.
I can use force trip function from TMS320F28379D to make ePWMxA and ePWMxB OFF But its not reflecting on the output of DRV3201.
Note :
I am using 6-pwm mode in DRV3201.
Configuration through SPI for DRV: SPIHAL_WriteRegister(CFG0,0x38);
SPIHAL_WriteRegister(CFG1,0x84);
Need help.
Anyone suggest is it possible to make both GHSx and GLSx OFF in DRV3201 ?
Thank you.