Other Parts Discussed in Thread: LAUNCHXL-F28379D
Hello,
I am using LAUNCHXL-F28379D board with Matlab/Simulink to build can communication. I want to use two can modules A and B. But i am little confused.
When I configured the eCAN transmit block as module eCAN_B and deploy the simulink model on the board, I was able to receive related can message (279) from CAN H/L pins (J12) on the board.
However,
When I configured the eCAN transmit block as module eCAN_A, I was not able to receive the message from the CAN H/L pins (J12).
I also could not understant that which pins on the board belongs to module eCAN-A or eCAN-B. It seems that GPIO31 and GPIO30 pins are responsible for eCAN-A , GPIO12 and GPIO17 for eCAN-B according to hardware board settings in configuration parameters. However I can not also receive the can message from that pins. I jusj was able to receive the message from J12 by configuring the eCAN transmit block module eCAN-B.
Do i have to change some parameters to work also with eCAN-A?
Thans in advance.
Birol