Part Number: TMDSCNCD28379D
Tool/software: Code Composer Studio
Hello everyone,
I am currently facing some problems with the connection between the DSP and my computer. The environment that I am running the DSP is quite noisy (EMI), however, I was wondering if there is anything that I can do regarding communication settings that may make the communication more immune to noise, even if it means a slower communication. Additionally, every time that I lose connection I am not able to connect back again unless I reload the code. Is it possible to reconnect to the DSP without having to reload the code?
Does anyone know how the DSP loses connection? Is that because of a series of packages that are corrupted? Is it because of the communication clock gets messed up? I have no clue how it works.
Right now, I generally use the dual graph to plot some data while running the code. Do you know if plotting too much data while the system is running can make the communication more susceptible to noise?
I apologize for the number of questions, but I appreciate any help even if it does not cover all of them.
Thank you,
Renato