This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with ADC-Measurement with TMS320F2812

Hi

I use the ezdsp-board f2812 together with matlab-simulink in order to produce code for the dsp.

In a small application I want to read at one of the adc-channels.

Unfortunately when i debug the assigned adc-register i read 0x8000>>4= 2048. This result is indepentend

of the input signal.

Do you have any idea?

With regards

Chris