Sometimes DSP F28335 hangs up while powering up, please see below schematic for the power on reset . While DSP hangs up I measured the RESET signal (output of U28) by probing at pin 4of the U28 NAND gate. It was 3.3 Volts. I also measured the input signals to that NAND. They were Pin 2 = 5 Volts, Pin 4 = 3.3 Volts.
Watchdog is disabled.
Please find the Power circuitry image attached.