This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28375S: TMS320F28375 cannot connect XDS110

Part Number: TMS320F28375S
Other Parts Discussed in Thread: TMS320F28075

Tool/software: Code Composer Studio

Dear,

we just use TMS320F28075 and to try connect XDS110, but not working.

and we catch log file

--------------------------------------------------------------------------------------------------------------------------------------------------------------

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\IVANCH~1\AppData\Local\TEXASI~1\
    CCS\ti-2\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Nov 21 2018'.
The library build time was '00:08:45'.
The library package version is '8.0.903.2'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

[End: Texas Instruments XDS110 USB Debug Probe_0]

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

If any suggestion, Please advise me.

Thanks,

Best regards,

Lawrence.

  • Hi Lawrence,

    It look like a board issue. I am assuming you are using custom board. Please check the signal integrity for all JTAG signals from device to JTAG header.

    Regards,

    Vivek Singh

  • Were you able to check the board to see if there is any issue with connection and fix it?

    Vivek Singh

  • Hi, Vivek Singh

    we try to JTAG setting low speed, to connect, but also fail.

    error log file.

    [Start: Texas Instruments XDS110 USB Debug Probe_0]
    
    Execute the command:
    
    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
    
    [Result]
    
    
    -----[Print the board config pathname(s)]------------------------------------
    
    C:\Users\IVANCH~1\AppData\Local\TEXASI~1\
        CCS\ti-2\0\0\BrdDat\testBoard.dat
    
    -----[Print the reset-command software log-file]-----------------------------
    
    This utility has selected a 100- or 510-class product.
    This utility will load the adapter 'jioxds110.dll'.
    The library build date was 'Nov 21 2018'.
    The library build time was '00:08:45'.
    The library package version is '8.0.903.2'.
    The library component version is '35.35.0.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '5' (0x00000005).
    The controller has an insertion length of '0' (0x00000000).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.
    
    -----[Print the reset-command hardware log-file]-----------------------------
    
    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the XDS110 with USB interface.
    The link from controller to target is direct (without cable).
    The software is configured for XDS110 features.
    The controller cannot monitor the value on the EMU[0] pin.
    The controller cannot monitor the value on the EMU[1] pin.
    The controller cannot control the timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '0' (0x0000).
    
    -----[An error has occurred and this utility has aborted]--------------------
    
    This error is generated by TI's USCIF driver or utilities.
    
    The value is '-230' (0xffffff1a).
    The title is 'SC_ERR_PATH_MEASURE'.
    
    The explanation is:
    The measured lengths of the JTAG IR and DR scan-paths are invalid.
    This indicates that an error exists in the link-delay or scan-path.
    
    [End: Texas Instruments XDS110 USB Debug Probe_0]
    

    if any suggestion, Please advise me.

    Thanks,

    Best regards,

    Lawrence.

  • Lawrence,

    If there is board issue, reducing speed may not help. You need to check the signal integrity of all JTAG signal from header to device.

    Regards,

    Vivek Singh

  • Hi Lawrence,

    Were you able to do signal integrity check for all the JTAG signals on the board?

    Regards,

    Vivek Singh